cancel
Showing results for 
Search instead for 
Did you mean: 

VL53L0X API Status: -6 : Range error. I developed a little instrument using VL53L0X to measure a distance ranging from 30 to 200 mm. We assembled 200 pcs and on 50% of them I get the error above, while the remaining 50% work fine. Anybody can help me?

GBern
Associate

API Status: -6 : Range error

===============================

//my code

.....

  if(Status == VL53L0X_ERROR_NONE)

  {

  //   printf ("Call of VL53L0X_StaticInit\n");

    Status = VL53L0X_StaticInit(pMyDevice); // Device Initialization

    print_pal_error(Status);

  }

  

  if(Status == VL53L0X_ERROR_NONE)

  {

  //   printf ("Call of VL53L0X_PerformRefCalibration\n");

    Status = VL53L0X_PerformRefCalibration(pMyDevice,

     &VhvSettings, &PhaseCal); // Device Initialization

    print_pal_error(Status); //-> API Status: -6 : Range error

  }

.....

VL53L0X_Error VL53L0X_PerformRefCalibration(VL53L0X_DEV Dev, uint8_t *pVhvSettings,

uint8_t *pPhaseCal)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

LOG_FUNCTION_START("");

Status = VL53L0X_perform_ref_calibration(Dev, pVhvSettings,

pPhaseCal, 1);

//Status = 0xFA

LOG_FUNCTION_END(Status);

return Status;

}

VL53L0X_Error VL53L0X_perform_ref_calibration(VL53L0X_DEV Dev,

uint8_t *pVhvSettings, uint8_t *pPhaseCal, uint8_t get_data_enable)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

uint8_t SequenceConfig = 0;

/* store the value of the sequence config,

* this will be reset before the end of the function

*/

SequenceConfig = PALDevDataGet(Dev, SequenceConfig);

/* In the following function we don't save the config to optimize

* writes on device. Config is saved and restored only once. */

Status = VL53L0X_perform_vhv_calibration(

Dev, pVhvSettings, get_data_enable, 0);

//Status = 0xFA

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_perform_phase_calibration(

Dev, pPhaseCal, get_data_enable, 0);

if (Status == VL53L0X_ERROR_NONE) {

/* restore the previous Sequence Config */

Status = VL53L0X_WrByte(Dev, VL53L0X_REG_SYSTEM_SEQUENCE_CONFIG,

SequenceConfig);

if (Status == VL53L0X_ERROR_NONE)

PALDevDataSet(Dev, SequenceConfig, SequenceConfig);

}

return Status;

VL53L0X_Error VL53L0X_perform_vhv_calibration(VL53L0X_DEV Dev,

uint8_t *pVhvSettings, const uint8_t get_data_enable,

const uint8_t restore_config)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

uint8_t SequenceConfig = 0;

uint8_t VhvSettings = 0;

uint8_t PhaseCal = 0;

uint8_t PhaseCalInt = 0;

/* store the value of the sequence config,

* this will be reset before the end of the function

*/

if (restore_config)

SequenceConfig = PALDevDataGet(Dev, SequenceConfig);

/* Run VHV */

Status = VL53L0X_WrByte(Dev, VL53L0X_REG_SYSTEM_SEQUENCE_CONFIG, 0x01);

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_perform_single_ref_calibration(Dev, 0x40);

//Status = 0xFA

/* Read VHV from device */

if ((Status == VL53L0X_ERROR_NONE) && (get_data_enable == 1)) {

Status = VL53L0X_ref_calibration_io(Dev, 1,

VhvSettings, PhaseCal, /* Not used here */

pVhvSettings, &PhaseCalInt,

1, 0);

} else

*pVhvSettings = 0;

if ((Status == VL53L0X_ERROR_NONE) && restore_config) {

/* restore the previous Sequence Config */

Status = VL53L0X_WrByte(Dev, VL53L0X_REG_SYSTEM_SEQUENCE_CONFIG,

SequenceConfig);

if (Status == VL53L0X_ERROR_NONE)

PALDevDataSet(Dev, SequenceConfig, SequenceConfig);

}

return Status;

--- 

VL53L0X_Error VL53L0X_perform_single_ref_calibration(VL53L0X_DEV Dev,

uint8_t vhv_init_byte)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_WrByte(Dev, VL53L0X_REG_SYSRANGE_START,

VL53L0X_REG_SYSRANGE_MODE_START_STOP |

vhv_init_byte);

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_measurement_poll_for_completion(Dev);

//Status = 0xFA

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_ClearInterruptMask(Dev, 0);

if (Status == VL53L0X_ERROR_NONE)

Status = VL53L0X_WrByte(Dev, VL53L0X_REG_SYSRANGE_START, 0x00);

return Status;

}

---

VL53L0X_Error VL53L0X_measurement_poll_for_completion(VL53L0X_DEV Dev)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

uint8_t NewDataReady = 0;

uint32_t LoopNb;

LOG_FUNCTION_START("");

LoopNb = 0;

do {

Status = VL53L0X_GetMeasurementDataReady(Dev, &NewDataReady);

//Status = 0xFA   

if (Status != 0)

break; /* the error is set */

if (NewDataReady == 1)

break; /* done note that status == 0 */

LoopNb++;

if (LoopNb >= VL53L0X_DEFAULT_MAX_LOOP) {

Status = VL53L0X_ERROR_TIME_OUT;

break;

}

VL53L0X_PollingDelay(Dev);

} while (1);

LOG_FUNCTION_END(Status);

return Status;

}

---

VL53L0X_Error VL53L0X_GetMeasurementDataReady(VL53L0X_DEV Dev,

uint8_t *pMeasurementDataReady)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

uint8_t SysRangeStatusRegister;

uint8_t InterruptConfig;

uint32_t InterruptMask;

LOG_FUNCTION_START("");

InterruptConfig = VL53L0X_GETDEVICESPECIFICPARAMETER(Dev,

Pin0GpioFunctionality);

if (InterruptConfig ==

VL53L0X_REG_SYSTEM_INTERRUPT_GPIO_NEW_SAMPLE_READY) {

Status = VL53L0X_GetInterruptMaskStatus(Dev, &InterruptMask);

//Status = 0xFA     

   

if (InterruptMask ==

VL53L0X_REG_SYSTEM_INTERRUPT_GPIO_NEW_SAMPLE_READY)

*pMeasurementDataReady = 1;

else

*pMeasurementDataReady = 0;

} else {

Status = VL53L0X_RdByte(Dev, VL53L0X_REG_RESULT_RANGE_STATUS,

&SysRangeStatusRegister);

if (Status == VL53L0X_ERROR_NONE) {

if (SysRangeStatusRegister & 0x01)

*pMeasurementDataReady = 1;

else

*pMeasurementDataReady = 0;

}

}

LOG_FUNCTION_END(Status);

return Status;

}

---

VL53L0X_Error VL53L0X_GetInterruptMaskStatus(VL53L0X_DEV Dev,

uint32_t *pInterruptMaskStatus)

{

VL53L0X_Error Status = VL53L0X_ERROR_NONE;

uint8_t Byte;

LOG_FUNCTION_START("");

Status = VL53L0X_RdByte(Dev, VL53L0X_REG_RESULT_INTERRUPT_STATUS, &Byte);

*pInterruptMaskStatus = Byte & 0x07;

//Byte = 0x48, 0x4C 

if (Byte & 0x18)

Status = VL53L0X_ERROR_RANGE_ERROR;

LOG_FUNCTION_END(Status);

return Status;

}

   

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.