2020-09-04 12:51 PM
I'm using the STEVAL-MKI109v3 demo board with the STEVAL-MKI193 IMU. I'd like to evaluate use of the FIFO. I've written a custom PC application based on the Unico Lite demo application. I can read from the FIFO registers properly, but it is really slow. It takes 2-3 seconds to read the entire 3k FIFO. How do I read the FIFO faster?
I've notice the "STMicroelectronics Virtual COM Port" driver defaults 9600bps. This could be the problem.
Thank you.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.