2019-12-09 4:04 AM
I am using LIS2HH12 with Atmel ATSAM4E8C and am able to read registers and write to registers.
When I read FIFO_SRC register (0x2F) I get Bit EMPTY=1 and in STATUS register (0x27) ZYXDA is constantly 0. I am following the example from https://github.com/STMicroelectronics/STMems_Standard_C_drivers/blob/master/lis2hh12_STdC/example/read_data_simple.c and has tried to enable FIFO in CTRL3 register (0x22) and FIFO_CTRL register (0x2E), but still no data in FIFO.
Is there any setup steps I am missing?
2019-12-11 6:35 AM
Hi @Philip Jönsson , unfortunately there are no LIS2HH12 example related to the FIFO directly available on Github repository. So I suggest you to take inspiration from the Lis3dh examples for the multi-read FIFO, because the control registers of the FIFO in the two cases are the same. I also suggest you to compare your code with p.34 and sgg of the AN4662. Regards
void example_main_lis3dh_fifo(void)
{
/*
* Initialize mems driver interface
*/
stmdev_ctx_t dev_ctx;
dev_ctx.write_reg = platform_write;
dev_ctx.read_reg = platform_read;
dev_ctx.handle = &hi2c1;
/*
* Initialize platform specific hardware
*/
platform_init();
/*
* Check device ID
*/
lis3dh_device_id_get(&dev_ctx, &whoamI);
if (whoamI != LIS3DH_ID)
{
while(1)
{
/* manage here device not found */
}
}
/*
* Enable Block Data Update
*/
lis3dh_block_data_update_set(&dev_ctx, PROPERTY_ENABLE);
/*
* Set Output Data Rate to 25 hz
*/
lis3dh_data_rate_set(&dev_ctx, LIS3DH_ODR_25Hz);
/*
* Set full scale to 2 g
*/
lis3dh_full_scale_set(&dev_ctx, LIS3DH_2g);
/*
* Set operating mode to high resolution
*/
lis3dh_operating_mode_set(&dev_ctx, LIS3DH_HR_12bit);
/*
* Set FIFO watermark to 25 samples
*/
lis3dh_fifo_watermark_set(&dev_ctx, 25);
/*
* Set FIFO mode to Stream mode: Accumulate samples and
* override old data
*/
lis3dh_fifo_mode_set(&dev_ctx, LIS3DH_DYNAMIC_STREAM_MODE);
/*
* Enable FIFO
*/
lis3dh_fifo_set(&dev_ctx, PROPERTY_ENABLE);
while(1)
{
uint8_t flags;
uint8_t num = 0;
/*
* Check if FIFO level over threshold
*/
lis3dh_fifo_fth_flag_get(&dev_ctx, &flags);
if (flags)
{
/*
* Read number of sample in FIFO
*/
lis3dh_fifo_data_level_get(&dev_ctx, &num);
while (num-- > 0)
{
/*
* Read XL samples
*/
lis3dh_acceleration_raw_get(&dev_ctx, data_raw_acceleration.u8bit);
acceleration_mg[0] =
lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[0]);
acceleration_mg[1] =
lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[1]);
acceleration_mg[2] =
lis3dh_from_fs2_hr_to_mg(data_raw_acceleration.i16bit[2]);
sprintf((char*)tx_buffer, "Acceleration [mg]:%4.2f\t%4.2f\t%4.2f\r\n",
acceleration_mg[0], acceleration_mg[1], acceleration_mg[2]);
tx_com(tx_buffer, strlen((char const*)tx_buffer));
}
}
}
}
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.