2019-07-16 11:49 PM
Hi,
I am using LIS3DSH Vibration Mems sensor in our project, we need temperature value from sensor. When I read OUT_T register in LIS3DSH , I am getting 0xFE from sensor.
Can, You tell how to decode this value temperature value.
Regards,
chaitanya
2019-07-16 11:53 PM
I am passing temperature value to twos complement function, I am getting 254, following is the function
int16_t two_compl_to_int16(uint16_t two_compl_value)
{
int16_t int16_value = 0;
/* conversion */
if (two_compl_value > 32768) {
int16_value = (int16_t)(-(((~two_compl_value) & (uint16_t)(0xFFFF)) + (uint16_t)(1)));
} else {
int16_value = (int16_t)(two_compl_value);
}
return int16_value;
}
2019-07-22 6:38 AM
Hi @chaitanya chippada , please consider that for LIS3DSH the temperature is on 8-bit, two's complement, so the function should be something like int8_t two_compl_to_int8. To get the actual temperature value, please consider that the resolution is 1 LSB/deg and 00h corresponds to 25 degrees Celsius. This means that if you read FEh, there will be 25°C + FEh = 25°C - 2°C = 23°C. Is the value FEh changing when you heat the sensor e.g. with a finger? Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.