2021-12-29 8:00 AM
Hi.
I bought a STEVAL-STWINKT1B board, however I try to perform all the steps to be able to see the data collected by the sensors and I can't because I can't understand what I need to do. I just wanted to connect this board via usb to my pc , monitoring data and saving it to a file (eg .txt) or saving the data to the sd card.
Can someone help me, please?
Thank you.
Solved! Go to Solution.
2022-01-05 5:51 AM
Hi @Tiago F , the STSW-STWINKT01 firmware package and in particular the HSDatalog example of the FP-SNS-DATALOG1 software package allows you to save data from any combination of sensors and microphones configured up to their maximum sampling rate. Sensor data are stored on a micro SD Card, SDHC (Secure Digital High Capacity) formatted with the FAT32 file system, or can be streamed to a PC via USB.
You can find the details in this document, p.26 and 27:
Here there is a tutorial on how to program the FP-SNS-DATALOG1 on the STWIN with STM32CubeProgrammer
2022-01-05 5:51 AM
Hi @Tiago F , the STSW-STWINKT01 firmware package and in particular the HSDatalog example of the FP-SNS-DATALOG1 software package allows you to save data from any combination of sensors and microphones configured up to their maximum sampling rate. Sensor data are stored on a micro SD Card, SDHC (Secure Digital High Capacity) formatted with the FAT32 file system, or can be streamed to a PC via USB.
You can find the details in this document, p.26 and 27:
Here there is a tutorial on how to program the FP-SNS-DATALOG1 on the STWIN with STM32CubeProgrammer
2022-01-06 1:49 AM
Hello @JWu.12 ,
Thank you very much!!
Best regards.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.