2019-10-17 2:27 PM
Hi,
The datasheet says the device is capable of SPI MODE 0 and 3, the default mode is 3. How does one change it to SPI MODE 0? Is it a hardware or software change?
Thanks.
2019-10-18 6:31 AM
Hi @DLim.16 , the change between the two SPI modes depends on the Master SPI (for example, an STM32 MCU), because it is basically related to the CS, CLK and MOSI reciprocal phases that are managed by the master, and the slave device will respond accordingly to the instruction received. Regards
2019-10-18 9:40 AM
Hi Eleon,
Thanks for the answer! I have another quick question. What changes do I need to make in the software and hardware to make sure the device is in SPI mode? I can read it in I2c, but never in SPI mode. I verified the SPI clock pulses and that the chip select was low during a spi transaction, and the serial output data was also correct, but I am not reading the correct data back. I am using STEVAL-MKI197v1 by the way.
Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.