2020-05-05 1:21 AM
2020-05-05 10:08 AM
Hi @Rrome.1 , the STEVAL MKI022V1 is a nrnd (no more supported) kit that should be equipped with a dedicated CD with a GUI that runs on Windows XP OS. Did you already tried to install the SW on Win7? Regards
2020-05-06 5:19 AM
hi,
yes I tried to install it, the software would seem compatible with W7/64, the problem is the device driver, I assumed that ST in the meantime had developed the driver for 64bit system.
thanks
2020-05-06 6:44 AM
Hi @Rrome.1 , adding STM32 topic which is fitting more the request. I see that the STEVAL MKI022V1 mounts an ST7 microcontroller and that the related drivers are limited to Win XP OS. You could try to install these USB drivers for ST LINK (STSW-LINK009) and check if it works... Regards
2020-05-08 9:33 AM
thanks for your answer, I tried the STSW-LINK009 driver but unfortunately it didn't work.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.