2023-03-03 12:07 PM
2023-03-03 12:50 PM
The Terms of Use do not specify an mcu to be used, but software support can only be provided by STMicroelectronics for its own mcu.
Does it answer your question?
Regards
/Peter
2023-03-03 1:22 PM
If I specify the feature, Could STM provide the convenient MCU- sensor module? As a sensor, I plan to use range finder sensor, optical flow sensor, 4 load cells, 2 linear encoders, 2 rotary encoders, 1 H- Driver and Bluetooth module for serial communication. If St provides this system to use, I can go with ST products.
Regards,
Fehmi Karaalioglu.
2023-03-06 5:12 AM
ST has many boards with very powerful and/or very low power MCUs. Depending on the interface of the range finder, the optical flow sensor, the load cells, the linear encoder and the rotary encoder, there will certainly be something for this application. Which interfaces are we talking about?
Regards
/Peter
2023-03-06 5:20 AM
in terms of MCU's power, we want around 100 Hz for our application considering all components works together.
2023-03-06 6:43 AM
That shouldn't be a problem.
Regards
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.