2017-09-01 8:29 PM
Hi there, I am currently running 4 LIS3DH chips in SPI configuration, outputting accel data @ 12bit (high res) 200Hz, +/- 2gs configuration.
The chips are not moving, and I noticed from the serial output terminal that the x,y,z acceleration value fluctuates in random intervals. The fluctuation applies throughout all of the LIS3DH chips, and is consistently scaled (up/down) by 2 on all acceleration axes output, in the same set of readings.
(e.g. x:1.01 y:-0.06 z:9.50m/s^2 fluctuates to x:2.09 y:-0.25 z:19.08m/s^2 in the next data set).
The raw value seems have this pattern of fluctuation as well (scaled by 2). (e.g. z raw: 15936 to 31424).
The code I am using can be found at
https://github.com/adafruit/Adafruit_LIS3DH
(Adafruit_LIS3DH.cpp).Am I missing something? Thank you.
#outputs #lis3dh #fluctuates2017-10-20 5:31 PM
Anyone have anything similar, or any experience on resolving this?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.