2017-12-15 11:25 AM
Hi, I'm working with a LSM6DSMTR device connected via I2C to a Nordic Semi nRF52382. I would like to use the FIFO feature and have a question about the address rounding:
If I start the multiple data read at the FIFO_STATUS1 register and read 154 bytes, would that read the 4 bytes of status registers and 150 bytes of FIFO data? Or does the first address have to be the FIFO_DATA_OUT_L register in order for the rounding to take effect?
#rounding #fifoSolved! Go to Solution.
2017-12-20 1:56 AM
I think you can start with FIFO_STATUS1 it should work.
2017-12-20 1:56 AM
I think you can start with FIFO_STATUS1 it should work.
2018-01-10 11:49 AM
I agree based on what I'm seeing on my HW. Thanks.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.