2021-01-29 7:54 AM
I cannot decide which one to use in my application, which is a portable radar fixed to the back of a vehicle. My only requirement is that its orientation is correct when first put in place. Will the LIS2DH12 suffice. I do know that the LIS2DW12 has better resolution, lower operating and sleep current, better sensitivity, higher frequency response. But I'm not sure if I need all the improvements it offers which come at a premium.
2021-01-29 8:34 AM
I'm also looking at LIS2HH12, out of these the LIS2DW12 is considerably more expensive than the others mentioned here. Looking at RS components we have the following price for 50 pieces;
LIS2DW12 £1.45
LIS2HH12 £0.84
LIS2DH £0.89
LIS2DH12 £0.92
2021-02-01 12:25 AM
Hi @TMahm.2 ,
So you basically need to detect a 4D / 6D orientation (or position) of your vehicle, and not the exact "real-time" tilt of it, or automotive-graded safety flags, right?
If so, as reference implementation, you can check the application note AN4662 p.31, where this feature is described.
In this case, the LIS2HH12 device should be enough, since this digital application is conceptually similar on all the devices you reported.
If you want a sample code showing this feature implementation, you can get an insight in the file lis2dw12_orientation.c: registers to be set are different, but structure is similar.
-Eleon
2021-02-12 2:57 AM
Hi @TMahm.2 ,
did you find the right solution for your application at the end?
-Eleon
2021-02-12 3:42 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.