2021-06-24 10:36 AM
Hi Sir,
We have used the LSM6DS3 part in our application boards. Now the distributor mentioned LSM6DS3 part ha end of life and New part is LSM6DSL.
Please confirm this new LSM6DSL part is pin to pin and firmware side compatible with the LSM6DS3 part. Or please share changes .
Regards
Anees PK
Solved! Go to Solution.
2021-06-25 6:08 AM
Hi Anees @APK.1 ,
LSM6DS3 and LSM6DSL are pin-to-pin compatible, as you can also see from the two datasheets, p.17.
LSM6DSL has some additional registers, such as the user offset compensation and the Bank B embedded function registers, and is in general more performant, so no issue also on firmware / software side.
You can check in this case the configuration C code on Github, lsm6ds3_read_data_polling.c and lsm6dsl_read_data_polling.c: in the LSM6DSL case, the configuration of internal filters is added, but it is not mandatory.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-06-25 6:08 AM
Hi Anees @APK.1 ,
LSM6DS3 and LSM6DSL are pin-to-pin compatible, as you can also see from the two datasheets, p.17.
LSM6DSL has some additional registers, such as the user offset compensation and the Bank B embedded function registers, and is in general more performant, so no issue also on firmware / software side.
You can check in this case the configuration C code on Github, lsm6ds3_read_data_polling.c and lsm6dsl_read_data_polling.c: in the LSM6DSL case, the configuration of internal filters is added, but it is not mandatory.
If my reply answered your question, please click on Select as Best at the bottom of this post. This will help other users with the same issue to find the answer faster.
-Eleon
2021-07-07 6:00 AM
Hi @APK.1 ,
any feedback about this?
-Eleon
2021-07-07 6:05 AM
Dear Eleon,
Thanks for the replay.,
I will check with the one sample new part ic .
Regards
Anees PK.
2021-09-07 2:06 AM
Dear Eleon,
I have tested the new sample with the existing code. It is working well, without make any changes in the code and design.
Thanks for the support.
Regards
Anees PK.
2021-09-07 2:08 AM
That's great! Thank you for your feedback Anees PK @APK.1
If you want, you can click on Select as Best at my first comment to your post. This will help other users with the same issue to find the answer faster.
-Eleon
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.