2014-05-22 12:08 AM
Is there more detailed spec on the temperature sensing of this part? In the data sheet it states +/- 2C from 0-80C. Is there a range where it is tighter?
We are finding that room temp (~25C) we are on the high end +1.4C to + 1.7C on many of the production units. This is ''within spec'', but I'm wondering if it should be tighter at room temp. We have other temp sensors on the same board which do have a tighter spec of +/- 0.5C at room temp, but then go up to +/-2C at –40C and + 120C.
</p>
Also, we are seeing that the pressure sensor does not provide temperature values below about –25C, is this expected? The operating temp should be down to –40C.
</span>
2014-10-06 7:27 AM
Hello,
Indeed the LPS331AP data sheet specifies 2 different parameters:
Top = Operating Temperature Range , - 40
°C
to 85
°C
that represents the temperature range physically supported by the sensor package .
Tfull = Full Accuracy Temperature Range, 0 to 80
°C,
that represents the temperature range where we provide specifications on temperature and pressure accuracy.
therefore Tfull is the right temperature range you have to consider for your developments.
Best RegardsWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.