2024-08-13 11:53 PM
Hello,
we're considering to use ASM330LHB in the SIL2 functional safety application and we would like to use and take credit from ST's ASILB-LIBRARY. However ASILB-LIBRARY use-case as it's documented expects that two redundant senors will be employed. Can be ASILB-LIBRARY used only with single IMU source?
Thank you for the answer and support
@Denise SANFILIPPO thank you for your awesome article on this topic https://community.st.com/t5/mems-and-sensors/how-to-augment-your-automotive-safety-applications-with-the-imu/ta-p/670346
Solved! Go to Solution.
2024-08-14 6:53 AM
Hi @KSzurman ,
Welcome to ST Community!
The ST ASIL B solution is made up of an ASIL B software library called ASM330LHBxx_ASILB_library, certified by the third party TÜV, and two identical IMUs (either 2x ASM330LHB or 2x ASM330LHBG1).
The ASIL B software library implements software safety mechanisms which allows the overall solution, which is made up of hardware (two redundant IMUs) + software library, to be ASIL B compliant.
So ASILB-LIBRARY cannot be used only with single IMU.
2024-08-14 6:53 AM
Hi @KSzurman ,
Welcome to ST Community!
The ST ASIL B solution is made up of an ASIL B software library called ASM330LHBxx_ASILB_library, certified by the third party TÜV, and two identical IMUs (either 2x ASM330LHB or 2x ASM330LHBG1).
The ASIL B software library implements software safety mechanisms which allows the overall solution, which is made up of hardware (two redundant IMUs) + software library, to be ASIL B compliant.
So ASILB-LIBRARY cannot be used only with single IMU.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.