MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionFx Magnetometer calibration issue

Hello Everyone!!!I am using STM32F401CBU6 controller along with 2 sensors ie., (ISM330DLC & ISM303DAC) in my project. I have included motionfx library and getting Roll, Pitch, Yaw and Heading, but the heading is not getting calibrated and values are ...

FX_Run.PNG Init.PNG Mag_Calib.PNG
Anil3 by Associate III
  • 3383 Views
  • 2 replies
  • 0 kudos

L3GD20 and 072B-DISCO

I want to use the L3GD20 gyroscope on my development board. But I didn't understand what I should do and I couldn't find an example on the internet. I know it communicates via SPI, but I could not send or read data. Can you please help me in detail? ...

BNP_0-1722525903040.png
BNP by Associate
  • 1894 Views
  • 3 replies
  • 0 kudos

Roll value changes with Pitch

Hello Everyone!I am using ISM303DAC sensor in my project and facing an issue with Pitch value.  I have used MotionMC library and  calibrated the Magnetometer for heading. and also it got calibrated. As MotionEC_Run() function output consists of Euler...

Anil3 by Associate III
  • 1087 Views
  • 0 replies
  • 0 kudos

Resolved! Qvar array

Hi all,  Would it be possible to have an 8x8 array of capacitive pressure sensors connected to the Qvar pins by an analogue multiplexer.I would like the qvar to effectively scan across the sensing array. 

TKula by Associate
  • 1245 Views
  • 1 replies
  • 1 kudos

Resolved! LSM6DSV16X AN5755

Hi, it seems there is a typo in AN5755 at page 8 ch.4.2 it says: "Moreover, Qvar data can be stored in FIFO (by setting the QVAR_BATCH_EN bit to 1 in the COUNTER_BDR_REG1 (0Bh) register)". This statement doesn't apply to LSM6DSV16X, because it is not...

licio by ST Employee
  • 2102 Views
  • 1 replies
  • 0 kudos

Integration of the example code for ilps28qsw

Hello everyone,I want to connect my pressure sensor (ilps28qsw) and have written the code in C and using I2C. If I use the example code as in the following link, and do nothing else, it works. For example, if I pull the variables (see below) out of t...

Jens4 by Associate II
  • 2521 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.