To access data by another microcontroller.
Posted on February 16, 2012 at 19:31Is it possible to access 3-axis acceleration data by another board(32L-Discovery) without using the uc of the iNemo?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on February 16, 2012 at 19:31Is it possible to access 3-axis acceleration data by another board(32L-Discovery) without using the uc of the iNemo?
Posted on January 27, 2012 at 00:59Has anyone successfully compiled any of the iNemo/DFU code? If so, how did you do it?I've tried Atollic/eclipse, which wouldn't work because there's no project file and I couldn't seem to resolve the dependencies ...
Posted on January 26, 2012 at 23:23I can't get DFU or iNemo firmware code to compile with Atollic.The code seems to be a mess with changes to the standard libraries, etc.. Please create a project file for Atollic, or tune up the code so it will com...
Posted on October 03, 2011 at 10:32Hi! I want to write sensors output to the SD card. can someone plz help me how to do this? regards hunzai #sd-card
Posted on December 01, 2011 at 19:46How I can interpret the temperature data from the Gyroscope L3G4200D? I can't find anything about the OUT_TEMP Data reference �C. I know, the range is -40 to 85�C. #l3g4200d #mems #l3g4200d #support
Posted on December 20, 2011 at 20:27I am facing timing issue with lis3dh accelerometer in FIFO mode.Currently my ODR=25 Hz and I am reading FIFO on watermark threshold=30.As soon as I get watermark interrupt I read 196 (32*3*2)samples at 5 Mhz.Hence...
Posted on January 17, 2012 at 08:02Hi ST-team,i have downloaded the iNEMOEngine LI3 software. After the registration I get the link to download the file with the name: ''iNEMO_Suite_2.3.0_110913.zip''. When I try to open it I get an error message th...
Posted on December 29, 2011 at 11:04Hi,I intend to use several STeval-MKI109Vx structures, up to ten systems, simultaneously, andall of them ''wireless''. STM offers a wireless Bluetooth kit for connecting to STeval-MKI109V1.Is it possible to use up...
Posted on December 06, 2011 at 11:42Hi,I met this problem, iNemoand computerconnectionssuggested that ''could notdistinguish between USBdevices, '' First of all, I wanted to step through the code line by line with JLINK, under the RDI mode, But aft...
Posted on August 16, 2011 at 14:32Hello, Im facing a problem with the Inemo SDcard api. Iam able to read and write multiple blocks and single blocks but Im not able to erase the card. When I issue a command for erase and then read the block ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.