2012-01-26 3:59 PM
Has anyone successfully compiled any of the iNemo/DFU code? If so, how did you do it?
I've tried Atollic/eclipse, which wouldn't work because there's no project file and I couldn't seem to resolve the dependencies and incompatibilities with the standard library.I also tried IAR 6.30, which wouldn't work due to CMSIS version incompatibilities, which nobody I've seen can seem to resolve.So what gives? How the heck am I supposed to do anything with this code? Why aren't any of the supposedly ''supported'' toolchains actually supported?2012-02-14 12:30 AM
Hopefully ST will at some point actually support at least one compiler properly. But...
ST support provided me with the following workaround...Try the following procedure:1) Open the project with IAR 6.20 or later version.2) In the left tab, in the CMSIS folder, right click on core_cm3.c file and go to “optionâ€�, and check “Exclude from buildâ€� available on the left-up corner of the option window (see attached figure1) and then press ok.3) Open the project options (Project à Options or ALT+F7). In the “General Optionsâ€� category, go to the “Library Configuration tabâ€� and check the “Use CMSISâ€� in the CMSIS part (see Figure 2).4) Go to the “C/C++ Compilerâ€� category, and then on “Preprocessorâ€� tab. In the “Additional include directories: (one per line)â€� list, remove the following path: “$PROJ_DIR$\..\..\..\Common\STM32F10xFWLib\v3_3_0\Libraries\CMSIS\CM3\CoreSupport\â€�, and then press ok (see Figure3).5) Now you should be able to compile it without problems.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.