MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

unable to use SPI interface

Posted on June 07, 2013 at 08:41I am trying to access the LSM330DLC devie using the SPI interface without luck. I have religiously tried to follow instructions in the part data sheet to read the WHO_AMI_G register but the there is no output on the S...

bnp979 by Associate III
  • 737 Views
  • 0 replies
  • 0 kudos

pdm filter

Posted on June 04, 2013 at 10:14libPDMFilter_IAR.a Does LibPDMFilter_IAR.a in the STMF4 DISCORVERY  is used for all STM32 family? for example, Is LibPDMFilter_IAR.a used for STM32F1XX not STM32F4XX????

sojaewoo by Associate II
  • 990 Views
  • 0 replies
  • 0 kudos

LSM303DLHC stuck on -4096

Posted on May 07, 2013 at 18:05We have two LSM303DLHC on one board. Sometimes one of them appears to be stuck at -4096 on some axes. Even when I wave a magnet close to it doesn't change. The next day it's ok. The board was sitting on my desk all day...

dimitar by Associate II
  • 885 Views
  • 0 replies
  • 0 kudos

Please help using LSM330D

Posted on May 03, 2013 at 06:25I am trying to get a gyroscope raw data using I2C. DEN_G is connected to MCU's GPIO and I set the register to use level trigger mode. I think I2C slave address is correct because when I read WHO_AM_I_G register I get 2...

suriko by Associate
  • 1005 Views
  • 1 replies
  • 0 kudos

LSM303DLHC DRDY interrupt difficulties

Posted on April 23, 2013 at 19:05Greetings,I'm trying to bring up an LSM303DLHC and I'm having trouble getting any form of interrupt out of the device.I've taken an STEVAL-MKI119v1 and removed the MKI108v2 and jumpered it to my I2C bus.  I have Vdd ...

ste2e by Associate
  • 792 Views
  • 0 replies
  • 0 kudos

LSM330 Programming Guide

Posted on April 12, 2013 at 14:42Is there a programming guide for LSM330? If there is one, could some one please post the link for that? #lsm330dl

mojink by Associate
  • 877 Views
  • 0 replies
  • 0 kudos

LIS331HH detection

Posted on April 12, 2013 at 11:06Hello,Accorting to datasheet, LIS331HH accelerometer don't have register WHO_AM_I. Is it possible to read identification data from 0xF register? What is identification value of LIS331HH? I need detect this accelerome...

mircoo by Associate
  • 975 Views
  • 0 replies
  • 0 kudos

STEVAL-MKI115V1 Bluetooth module not working

Posted on April 08, 2013 at 22:36Hi all, I am new to the ST MEMS line, and recently purchased a few of the development boards to start testing (STEVAL MKI109V2, MKI120V1, and MKI115V1).  I followed the manuals for assembly and installing Unico, and ...

LIS3DH:Reading temperature from OUT_ADC_3_L, OUT_ADC_3_H

Posted on April 08, 2013 at 14:28Hi, I am trying to read temperature values from OUT_ADC_3_H. I have also enabled BIT 6 and 7 in TempCfgReg and  Block Data Update, BDU  at CTRL_REG4(0x23). CTRL_REG1 is set to 100 Hz with value 0x57 running in normal...

tbaddam9 by Associate
  • 840 Views
  • 0 replies
  • 0 kudos

LIS3DH SPI 3/4 wire not work properly

Posted on April 01, 2013 at 16:19Hello.I use LIS3DH accelerometer with 4-wire SPI interface.I attached schematic of accelerometer connection (AccelSch.pdf).ACL_VDDIO = 3,3 VACL_VDD = 3,3 VOther ACL signals connect to microcontroller pins.R9A=R9B=R9C...

maxim23 by Associate
  • 1744 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.