Simulation files for LPS22/25/331
Posted on January 05, 2017 at 00:51Are there any spice or cadence files to simulate the lps22h/25h/331ap pressure sensors to co-simulate them with an ASIC?If yes, how does one access them?Thanks
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Posted on January 05, 2017 at 00:51Are there any spice or cadence files to simulate the lps22h/25h/331ap pressure sensors to co-simulate them with an ASIC?If yes, how does one access them?Thanks
Posted on December 23, 2016 at 04:42I am a new user of ST’s LIS2DH12. I am confused about the sentence 'Leave “Pin 1 Indicator� unconnected during soldering'. It was in chapter 4.1 Soldering information in datasheet of LIS2DH12. What this sent...
Posted on December 29, 2016 at 15:42I'm trying to connect SPH0641LU4H-1 microphone to STM32F411RE Nucleo board.According to the Wikipedia https://en.wikipedia.org/wiki/Pulse-density_modulation format should represent lowest and highest amplitude as ...
Posted on December 21, 2016 at 11:26Hi, I am trying to configure osxmotion library in Juma Canon. I was able to successfully import motionar,motionfx,motioncp,motiongr library in the project but was unable to properly execute the license manager. I ...
Posted on December 30, 2016 at 08:14Here's my configuration:set(CTRL_REG1, 0x00); set(CTRL_REG2, 0x80); set(CTRL_REG3, 0x00); set(FIFO_CTRL, 0x00); //Flush FIFO set(CTRL_REG1, 0x3A); //3A was 3E set(CTRL_REG2, 0x50); //50 set(CTRL_REG3, 0x00); set(...
Posted on December 28, 2016 at 08:23I am designing circuit using LIS2DH12. I want to use the I2c, so I connect Cs to high level, and SA0 to GND. I am not sure if CS should be connected to Vdd, or Vdd_IO. As I understand it, Cs should be connected to...
Posted on December 05, 2016 at 20:44Hi.Sorry for my English.specified in the datasheet If a slave receiver does not acknowledge the slave address (i.e. it is not able to receive because it is performing some real-time function) the data line must be...
Posted on December 23, 2016 at 07:27Hi, I am new to LSM6DS3 inertial module, I am trying to use it with my arduino mega 2560, in SPI mode ,but in trouble with Z & Y axis output of the accelero meter. X axis output respond well.Already tried to read...
Posted on December 21, 2016 at 20:32Hi,I have connected an FPGA to an LPS331ap, and I can retrieve good data as seen in the oscilloscope, but only if the supply voltage is above 2.4V (I have Vdd and Vdd_io shorted together), rather than the 1.71V qu...
Posted on December 20, 2016 at 17:32I am using the LSM6DS3 component in a design. I've used the component in the past (and always liked it), but never in this capacity. I am using I2C for communication with 10k pull up resistors and am powering on/o...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.