MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LIS3DH accelerometer sensitivity in low power mode

Posted on July 17, 2015 at 15:05Hello,I am planning to operate the LIS3DH accelerometer in low power mode (resulting in an output data rate of 5kHz according to Table 26 in the datasheet).In Table 3 in the datasheet a sensitivity of 12mg/digit is gi...

stephan by Associate
  • 2424 Views
  • 3 replies
  • 0 kudos

LIS3DH 5kHz ODR not possible

Posted on May 09, 2016 at 15:33Hello all, I want to use the LIS3DH accelerometer and a Steval-MK1109v2 Motherboard with the ST Unico GUI for logging Acceleration data. The datasheet of the LIS3DH shows the possibility to meassure a bandwidth up to ...

www.st.com

Posted on August 11, 2017 at 19:00Hello,  I am trying to use the http://www.st.com/en/evaluation-tools/steval-mki129v1.html board on a breadboard.  It has a http://www.st.com/en/audio-ics/mp45dt02-m.html.  I am trying to resolve the two data sheets ...

0690X00000603hJQAQ.jpg 0690X000006040JQAQ.jpg 0690X000006040TQAQ.jpg

Resolved! MEMS pdm microphone - custom board

Posted on August 10, 2017 at 13:33Hi community!So far i have been developing my audio application on discovery board STM32F407 (there is a embedded MEMS microphone connected to I2S2), I have been able to configure I2S2 periphery and acquire data wit...

aci_gatt_update_char_value Failing For IDB05A1

Posted on August 06, 2017 at 20:02I have an IDB05A1 using aci_gatt_update_char_value. This call works for anything using 4 byte array sizes or smaller, but it returns BLE_STATUS_ERROR for arrays larger than this. I'm calling both aci_gatt_init and a...

hushel by Associate II
  • 794 Views
  • 0 replies
  • 0 kudos

State Machine programming for LSM330

Posted on February 15, 2017 at 06:13I am looking for some code examples or technical notes on programming the state machine in LSM330TR but couldn't find any in ST.com. Has anyone found these ? Could you please share if you have.#lsm330-state-machin...

iNemo-M1 Board

Posted on June 05, 2014 at 16:02Hi, I bought the iNemo-M1 Board.I connect it to PC by USB board, but PC not recognized the board.The board is aready programmed?I need to select an iNemo DFu firmware to program?Thanks.Eduardo Scherrer #inemo-m1-bo...

LIS2DS12 - Does Wake Up interrupt block other interrupts

Posted on August 01, 2017 at 21:23I'm trying to configure my LIS2DS12 accelerometer such that I can receive both wake and tap events. Whenever I enable (set the INT1_WU pin in ctrl4) I don't get tap events. I have three cases:1. enable just the wake...

Wrong pressure reading from LPS25HB sensor.

Posted on August 01, 2017 at 18:56Hi all,I am evaluating the LPS25HB pressure sensor on iMX6 host processor, I am interested in getting the altitude for our usecase.The problem is  I am getting consistent value of pressure with no change even when I...

Reducing accelerometer noise using sensor array?

Posted on July 27, 2017 at 18:53Hi to all, I was taking a look to LIS344ALH accelerometer for a project where I need to place MEMS accelerometer into Raspberry board.I've heard there is a way to reduce acceleration noise placing sensors in array (e....

mbertoni by Associate II
  • 2019 Views
  • 3 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.