2016-05-09 6:33 AM
Hello all,
I want to use the LIS3DH accelerometer and a Steval-MK1109v2 Motherboard with the ST Unico GUI for logging Acceleration data. The datasheet of the LIS3DH shows the possibility to meassure a bandwidth up to 5000Hz, which i need for my shaker meassurements. I used the Unico GUI to configure the Sensor at +-2g and the 5000Hz mode. I tried a 160Hz sine signal at the shaker and made an online FFT at the Unico GUI, but there was shown a peak at about ~600Hz, so i took a look at the logged data in the .txt-file. I wanted to add a timepath but recognised that the number of the lines weren�t right at all. I logged data at about 3 seconds but got only roundabout 4000 lines. With a ODR of 5000Hz i expected up to 16000 lines. I tested the modes with 400Hz and 1250Hz and both online-FFT an logged data were right. If I use the 0.0008s timesteps (1/1250Hz) for the logged 5000Hz-mode before, it looks right... So theres my question: Does the Unico GUI only logg data with a rate up to 1250Hz(even in the 5000Hz mode) or could it be a bug in the Unico GUI software? If I take a look on the wrong online FFT of the GUI, where 600Hz are shown but surely only a 160Hz-signal is given, it looks like that. Im a little confused. Thanks for your help! Greetings, Markus Schulz #lis3dh-odr-bandwidth-unico-gui2017-08-15 1:25 AM
Hi Markus,
I have the same question. Did you already make progress on this or have you switched to a different sensor? Would you be so kind to share your findings?
Kind regards,
Dave
2017-08-15 4:35 AM
Hi Dave,
can you please try the latest version of Unico software and FW for STEVAL-MKI109V2. Both you can find
.I tested it right now and I'm able to log data from LIS3DH at 5.376 kHz.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.