MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STPM10 Register reverse counting

Posted on November 22, 2017 at 06:19   We are working with STPM10 to measure the Voltage,current,Active energy,Reactive energy and apparent energy. we are using 10W to 1KW load.with current calibration as +12% and Voltage calibration as +9%. Upto 40...

LIS2DE12 Interrupt on INT2 pad

Posted on November 17, 2017 at 22:11I am unable to generate an interrupt on INT2 pin. But I can generate an interrupt with the same configuration on INT1 pin. Seems like I am missing something obvious or the datasheet is missing something crucial!!I...

LSM6DS33 => Fifo continous mode bad time values

Posted on November 18, 2017 at 16:03Hello everyone,I've problem with using Continous Fifo mode. During data processing I get periodically strange values in timestamp. In table below is shown configuration whitch I use.I use interrupt on fifo treshol...

Resolved! LSM6DSM FIFO not working

Posted on November 19, 2017 at 00:05I can't get the FIFO to work. The LSM6DSM is connected to a microcontroller via SPI. The sensor works fine when I use the status register and data registers to get the accel and gyro data.But for higher ODR I want...

LIS2DS12 positive self test values

Posted on November 17, 2017 at 22:41What is the expected self test difference values that should be expected? The spec indicates between 70 mg  and 1500 mg which seems like a very large range. Most other ST sensors has this value in a few hundred mg...

How to remove the spin from a sensor tile inside a baseball?

Posted on November 12, 2017 at 17:29I've added a sensor tile (STEVAL-STLKT01V1 SensorTile) inside of a baseball. How do I remove the spin of the base ball from effecting the accelerometer, gyro and magnetometer?I'm a beginner at this...Thank you,Ter...

Configuration of the Click recognition on the LSM9DS0

Posted on May 23, 2017 at 17:04Hi,  I am working with the Lsm9ds0 sensor and i would like to properly configure the Click recognition. After reading the datasheet I manage to rise an interrupt on a click but i still have a question about this functi...

0690X0000060752QAA.png

LIS3DH or LIS331H @ 4.2V ?

Posted on November 17, 2017 at 14:02Hello,I'm trying to design device with all components powered by li-po battery to minimize the power losses, cost and SIZE.I'd like to avoid voltage regulator, level shifters etc.This sensors should be powered up ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.