MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

LPS22HH I3C Address Assignment Collision

I'm working on a new design requiring four pressure sensors. The LPS22HH only allows two I2C address's through pin 5. Rather then increase complexity by putting all four on SPI I wanted to see if I could use the I3C bus capability. The datasheet refe...

STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0

I'm trying to evaluate STEVAL-MKI015V1 with STEVAL-MKI109V3 and Unico 7.0.0.0. The device appears in the selection menu, but I got the error "Device is not supported by the motherboard". I successfully completed the firmware upgrade through DFU (curr...

SROSS by Associate
  • 1092 Views
  • 1 replies
  • 0 kudos

I design a battery powered BT Tag using LIS3DE. I want to detect movement as a trigger to transmit BT beacons. Which mode should be choose if I want to reduce the power consumption.

LIS3DE connects to BLE IC using I2C Bus and INT pinsPlease state the mode according to time before and after the trigger.Second, if I want to monitor 30 seconds after trigger to double check is it need to transmit BT beacons. May I use LIS3DE FIFO to...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.