MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

IIS3DHHC

Dear Community,I am excited to get started with the IIS3DHHC sensor in combination with an Arduino Teensy. I have been working before with the Analog Devices ADXL355, I've successfully wrote a program for this, but I have difficulties knowing if I'm ...

CMull.81 by Associate
  • 1224 Views
  • 1 replies
  • 0 kudos

Size and position of Hall Plates in IIS2MDC Magnetometer

HelloI want to use the IIS2MDC magnetometer in a device which measures magnetic fields that change rapidly as a function of position (e.g. fields with high gradients). For this purpose, I need to know two things which i couldn't find in the datasheet...

Dvon by Associate
  • 1329 Views
  • 1 replies
  • 0 kudos

On the IIS328DQ, are the INT pins active high or low?

I am assuming that since they can be configured as push-pull or open drain that they are likely active low, but I would like to confirm this assumption. It seems odd that there is nothing in the datasheet about these pins -- only info about their sof...

Resolved! MotionFX Library ARM Cortex-M4F Hardware Floating Point

Hi,I am attempting to port the MotionFX Library example to another processor. The project I am using as a reference is the DataLogFusion project for the STM32L476RG-Nucleo in the X-CUBE-MEMS1 V6.0.1. I am trying to compile it on another ARM Cortex M4...

Daniel L by Associate III
  • 2429 Views
  • 4 replies
  • 0 kudos

Impact of regular self test on MEMS.

Hello everyone, I'm developing an IoT product with the LIS3DH and I'm thinking about running the self-test regularly this could be anything between 30 minutes and 2 hours; would this kind of behavior impact the life of the sensor? is there any data o...

Out of range readings of VL53L1X

Though the maximum range of the VL53L1X is 400cm, it gives random readings within 400cm when it is directed to open space. The VL53L0X gives a value about 8.1m for out of range measurements so that we can filter out them. But in VL53L1X there is no w...

TSura by Associate
  • 10692 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.