2019-04-16 6:43 AM
2019-04-30 6:05 AM
Hi, sorry for the delay in the answer. Which device are you using (accelerometer, 6axis...) and which part number? And which is you target application (e.g. is it an automotive application)? You can btw check the X-CUBE-MEMS1 and the related libraries (here). You could in general use the Motion AR library that enables the activity recognition function, but some sensor enables you to develop a Finite State Machine or a Machine Learning to implement the activity recognition. Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.