MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

lsm6dsv with lis2mdl sensor hub

HelloI would like to get the lis2mdl magnetometer data using the lsm6dsv second i2c line using the sensor hub.so far I get the accelerometer and gyroscope data via SPI and I want to add the magnetometer data.The code I have to configure the sensor hu...

Eddess by Associate II
  • 1241 Views
  • 1 replies
  • 0 kudos

Resolved! stuck trying to get STEVAL MKBOXPro connected

Hi I purchase a STEVAL MKBOXPro. It connects to phone and app fine but i'm having trouble to get the device connected to MEMS studio and Unicleo GUI  BLE Connection issue... 1. device manager detects STBOX but does not connect on MEMS studio and Unic...

khonsaiho by Associate II
  • 3435 Views
  • 9 replies
  • 2 kudos

LSM303AGR - distinguish required movement from noise

Hi,I'm developing a prototype based on an already existent product that contains an LSM303AGR, the goal is to install the device in a tower and detect when the tower is tilted or fallen, for this task the idea is to wake up the device via the interru...

A.Presm by Associate
  • 1063 Views
  • 2 replies
  • 2 kudos

Using the STM drivers with kernel above 6.6 i.e 6.13

Hi,im currently working on interfacing the STM mems sensors with Beagle Vahead board, im using a kernel version of 6.13 and i tried patching the STM MEMS IIO drivers from link. Im aware that the STM has confirmed the testing of the driver with kernel...

LIS2HH12- Tilt detection with interrupt

Hello everyone, I'm stuck and I need some help. I have the LIS2HH12 accelerometer connected to my raspberry pi via SPI. So far, I have been able to collect real-time accelerometer data . But my goal is to only get data once the accelerometer is title...

Resolved! STEVAL-MKI228KA arduino

Hello,Please , can i use the module STEVAL-MKI228KA (ILPS22QS) with arduino ?Thanks

ljm by Associate III
  • 1324 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.