VL53L0X sensor read not working
Hi,I try to read the VL53L0X sensor using the continuous read function. When I try to read the register 0x14 (result range status) + 10, I always get a fix value of 0x1FFF.
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi,I try to read the VL53L0X sensor using the continuous read function. When I try to read the register 0x14 (result range status) + 10, I always get a fix value of 0x1FFF.
Hello,We are encountering an issue using magnetometer function of a LSM303AGR.I2C line is OK, we can read WhoAmI register of both accelerometer and magnetometer using low level I2C functions. So we can retrieve accelerometer data without any problem ...
I configured LSM303AGR accelerometerit for high accuracy mode 50Hz and I am reading it at 20 Hz via i2c.The xyz signals are very unstable, and the final angle calculated (see figure) has huge variations. 2 degrees is far from what my expectations for...
Hi,I am quite new to MEMS IMUs. I have a custom board containing LSM303AGR IMU connected to SAMD21 MCU via I2C.I am using the stm32duino LSM303AGR library.I am having a hard time understanding the Self test procedure. Is it possible to get a simpler ...
Hello all,I've recently been trying to make the LSM6DSOX run ultra-low-power. However, I can't get it to work. I tried it with the 109V3 dev board in Unico, where I can get it to run at ~15uA. However, when I turn that configuration into a .h (header...
Hey all,I bought the STEVAL-BCN002V1B and need for my use case live sensor data of the accelerometer, gyroscope, magnetometer and the data of the senor fusion in MATLAB.I already tried the Unicleo software and the ST BLE Sensor-App, but i only found...
I have the SensorTile development kit, where I am able to successfully connect and use the SensorTile with either the cradle or expansion board. What I would like to do is use the SensorTile core board without having to use the cradle or the expansio...
I'm a studtendt from Beijing ,China. I want to use STTS75, an integrated digital temperature sensor and thermal watchdog in a high-g enviroment(~200g). Could someone tell me how the sensor works and its capabilty of bearing high acceleration? Pape...
LSM6 set to 2000 degrees/s feeding continuously to the FIFO at 208Hz. Solid synchronization on the data coming out of the FIFO. Stationary and at Constant 31 degrees C indicated, in 12500000 samples the average x-gyro reading has drifted from 607 to ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.