MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to use TIM with SPI to acquire audio data from MEMS microphone

Hello :smiling_face_with_smiling_eyes: I'm using the microphones on the X-NUCLEO-CCA02M2 Digital MEMS microphones expansion board based on MP34DT01-M for STM32 Nucleo. This card is plugged on nucleo stm32h743zi2My problem is that I have to interface ...

0693W000001sGcXQAU.png
UTANG.1 by Associate II
  • 9455 Views
  • 4 replies
  • 0 kudos

Resolved! re: ISM330DLC / LSM6DSM - reading FIFO

I need some help please re ISM330DLC – extracting data using FIFO_DATA_OUT_H and FIFO_DATA_OUT_L as described in AN5125 section 8.5.1.I don’t fully understand table 85. Where does the FIFO_PATTERN_[9:0] come from?How is the association between Next r...

CHarr.1 by Associate II
  • 2431 Views
  • 2 replies
  • 0 kudos

I am having a issue running LIS2DW12TR in 3V environment, the part is working fine at 1.8V once i plug the device to 3V supply it will start getting high current and some times burn.

we already cut trace the pin SDO connected to GND but still same issue, INT1&2 not connected physically by flipping MCU pin so it will not connect, the most ideal for our application is run the accel in 3V supply so we do not need a translator or any...

0693W000001s1jTQAQ.png
Jpena.1 by Associate
  • 1694 Views
  • 2 replies
  • 0 kudos

How to install VL53L3CX Linux driver into a linux system?

Dear ST-Team,I bought a VL53L3CX-SATEL board, but i didn't buy  X-NUCLEO-53L3A2 board. I have downloaded the Linux Driver "en.VL53L3CX_LinuxDriver.zip". I just followed the doc in the zip. Finally I found i can't access the i2c,the board did't work, ...

Wli.2 by Associate II
  • 1271 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.