MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is the accuracy of stm32f070 internal temperature sensor?

Hello,As per page number 17 of datasheet of STM32F070 series we can see that it consists of internal temperature sensor. It's written that with calibration we can get quite accurate value of the temperature but can it be used as replacement of any ex...

JKSah by Associate II
  • 3353 Views
  • 3 replies
  • 0 kudos

Resolved! will vl53l0x work in outdoors?

I performed all the calibrations indoor and whenever i am testing it in outdoor(both under direct sunlight and opposite) ,it is always detecting some particle without any interference.Do i need to perform calibrations again in outdoor?

ANANTH by Associate
  • 1514 Views
  • 1 replies
  • 0 kudos

Resolved! What is the ZERO offset value of LIS3DH after Factory Calibrated?

HI, After Factory calibration of LIS3DH accelerometer, what are the range of values given by the accelerometer( Selected 12 bit OUTPUT). I am getting 20-30 ADC counts of X axis from accelerometer, where as -1 to 3 counts from Y axis . Why there ...

NMale.1 by Associate III
  • 1641 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12 I2C write timeout

My application is very low power, and I need to save power wherever possible. To this end, I do the following:LIS2DE12_WriteReg(LIS2DE12_MEMS_I2C_ADDRESS, 0x20, 0x08);Which basically puts the accelerometer in power down mode. The LIS2DE12_WriteReg ba...

Resolved! lis3mdl connected to lsm6dsox I2C

Hello, support team.In my test board, lis3mdl is connected to lsm6dsox I2C.From above board, I want to read acceleration and gyro at 1667Hz, magnetic at 1kHz.I refer to lsm6dsox_sensor_hub_fifo_lis2mdl.c to implement SW.But It looks like magnetic da...

JPARK.2 by Associate II
  • 2150 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.