MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can I use the iNEMO ISM330DHCX on eval kit STEVAL-MKI210V1K for Sampling speed for Vibration Detector freqs 1k to 2.5khz.

I have a ISM330DHCX and evaluation kit for a vibration detector. Can the Unico / Weka Machine Learning Core work at above 104Hz? I've got a vibration class in the 1k -> 2.5k hz.  In Unico 'Options Tab' I can set the Output Data Rate to 6.66 kHz, bu...

dpeng by Associate
  • 1277 Views
  • 1 replies
  • 0 kudos

Resolved! Reading data from L3GD20 (SPI)

Hi,did anyone try to connect to the gyro (L3GD20) on F303Discovery board over SPI?I have a problem even with reading the WHO_AM_I register:My code is generated with Cube and I added the following lines:퐮퐢퐧퐭ퟖ_퐭 퐝퐚퐭퐚_퐰퐡퐨퐚퐦퐢, 퐚퐝퐝퐫퐞퐬퐬_퐰퐡퐨퐚퐦퐢;퐚퐝퐝퐫퐞퐬퐬_퐰퐡퐨퐚...

Ala1980 by Associate II
  • 15246 Views
  • 29 replies
  • 0 kudos

Gyroscope Sensors in different iPhone models

For our project at the THM in Germany we're developing an app which should help medical staff to detect parkinson symptoms via motion sensors in an early stage (for example by examining the rotation speed of the patients' hand etc.). Is it possible t...

MKirs.1 by Associate
  • 2038 Views
  • 1 replies
  • 0 kudos

No SPI response from ICM-20948 (IMU) on STM32

I have made a simple setup with 2 ICM-20948 IMU's and an AtSAMD21 MCU, which communicated through I2C and worked fine. Now I've chosen a more powerful MCU (STM32F410R8T6), and decided that a SPI setup would be advantageous. I have made the modificati...

0693W000005CumUQAS.png 0693W000005CumeQAC.png 0693W000005CumtQAC.png 0693W000005Cun8QAC.png
VSøby.1 by Associate III
  • 5538 Views
  • 4 replies
  • 1 kudos

lis3dsh Wakeup

hi stm,i have studied lis3dsh app note,i didn't understand complete configuration for wakeup state machine , like after setting the registers to the specific value , interrupt will be generated , how to make it periodic interrupt , what are all the t...

MKS by Associate II
  • 1155 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.