MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Now I am using LSM6DSO on my own board and using its embedded pedometer function. I want to do more custom change.

This pedometer function can count steps after the first ten steps.  The first ten steps is defalt and the application note said it can be change other value. I have found I should set up ****_DEB_STEPS_CONF register. But I don't know how to do that. ...

JXiao.1 by Associate II
  • 2433 Views
  • 8 replies
  • 0 kudos

Resolved! LIS3DH Single and Double click interrupt at the same time

Single click interrupt works fine, Double click interrupt works fine. When trying to enable both at the same time only the double clicks work. I have searched, and there are 3 old topics with this exact question, all are closed with no answer. Could ...

ELevh.2 by Associate II
  • 1979 Views
  • 2 replies
  • 0 kudos

Limitation of Unicleo-GUI to represent FFT data

We have designed custom board which has STM32F446RE MCU and ISM330DLC vibration sensor.We are able to send FFT data with 512 sample to Unicleo-GUI and able to observe the FFT data for X,Y,Z axis on graph.But when we send FFT data with 1024 samples t...

0693W000006F3FDQA0.png 0693W000006F3GBQA0.png
Rajesh1 by Associate II
  • 3503 Views
  • 7 replies
  • 0 kudos

LIS2DE12: help for configuring Stream to FIfo active on INT2

HI, I would like to use the LIS2DE12 to detect displacement (if someone moves my product from it starting place). As i should not be disturbed by vibration (workers, kick,…) I would like to do the detection in two steps :1)     Use INT2 to detect sma...

AGran.3 by Associate
  • 1687 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.