MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! If Hang up I2C interface of the LIS2DH

If Hang up I2C interface of the LIS2DH, How can i reset the device except VDD OFF/ON operation?I am considering to send 9-clocks to the SCL of the LIS2DH.

BBQ by Associate II
  • 1594 Views
  • 1 replies
  • 0 kudos

Sinc Filter Order and value output of DFSDM

Hello dear ST-Forum,I'm currently working on DFSDM and MEMS-Microphone and am trying out the sinc filters. By changing the filter order e.g. from filter order 1 to filter order 3, the values increase dramatically. I have not found any proper calculat...

crackl1ng by Associate III
  • 1676 Views
  • 1 replies
  • 0 kudos

we cannot use the interrupt in LPS27HHW!

We purchased the LPS27HHW chip from your company and we are testing it. Then, we found an abnormal situation about the threshold interrupt function. When the air pressure is higher than the threshold, the interrupt can be triggered properly, but it c...

Xxia.1 by Associate II
  • 1347 Views
  • 1 replies
  • 0 kudos

Trouble runing MotionGC_Update function.

Hi,I've been trying to get the calibration values for my gyroscope using MotionGC library. I'm using the sample code available in the MotionGC starter guide but the said function return all the output values as 0. The bias_update variable is also set...

PMach.1 by Senior
  • 8563 Views
  • 22 replies
  • 0 kudos

Resolved! possilbe inaccuracy at the sampling frequency for LIS2DS12

Hello ST community,I am interested in measuring the acceleration with two LIS2DS12 sensors at the same time. Therefore, I start the measurement (nearly at the same time) with a sampling frequency of 800Hz for 10 seconds with +-2g full scale range for...

LBaum.2 by Associate II
  • 7250 Views
  • 5 replies
  • 0 kudos

Resolved! DIfference between interrupt get and set

I was taking a look at this repository to get a bit used with the lis2dw12 accelerometer. Trying to use the Activity example I've got the expected results but got a bit confused with the routing of the detection to the interrupt pin. From line 185 on...

MRive.2 by Associate
  • 1258 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.