MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! What is STE150N10 replacement?

Hello, did ST ever made a STE150N10 direct (Drop in) replacement?if so, what would be the partnumber? thanks

GPirt.1 by Associate
  • 1263 Views
  • 1 replies
  • 0 kudos

Resolved! LSM303dlhc Accelerometer functionality not working

Hi ,After downloading the stm32f401 disco demo .hex file to the board, the accelerometer functionality is not working after pressing the user button as per the readme instructions. It means the LSM303dlhc chip is damaged.So to confirm that, will you ...

x-nucleo-iks01a2 with motionFX library

Hello,I'm using nucleoF446RE with X-NUCLEO-IKS01A2. I read data from sensor (LSM6DSL and LSM303AGR) and with MotionFX library I get rotations, but there are some problems.At beginning, if I don't rotate the board, the z-axis rotation is different fr...

AR1 by Associate II
  • 8851 Views
  • 8 replies
  • 0 kudos

I am using Sensortile/box STEVAL-MKSBOX1V1. I have connected the device using NUcleo F401RE board for realtime debugging. How I shall enable Virtual Com Port

I Have configured as shown in the picture , How should I enable the Virtual Com port,. My intention is evaluating all the sensors and push the data to Virtual COM Port. I am writing program for I2C_TempSensor - STTS22H  , for that I have configure fr...

0693W00000Czq9PQAR.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.