MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! footprint pattern to ASM330LHH?

Hi!Could yo tell me some information, where I can find footprint pattern to ASM330LHH device?Thanks for your help!

EMara.1 by Associate
  • 3169 Views
  • 3 replies
  • 0 kudos

Unico UCF file format

Hi,I am evaluating the LSM6DSOX sensor, focusing on the machine learning features. I have generated a UCF file using the Unico GUI, and I'd like to upload the configuration to the chip. I am using a custom board, not one of the official motherboards,...

Resolved! STEVAL-WESU1 battery not charging

Hello!I recently bought an STEVAL-WESU1 sensor unit. However, when I connected the USB cable to the circuit board, the on board RED LED keeps blinking. According to the documentation it should be steadily lit to indicate charging. Would you be able t...

TAswi.1 by Associate
  • 3212 Views
  • 6 replies
  • 0 kudos

lis2dtw12 Activity/Inactivity Sensitivity & Full range, etc

Using the ST Micro github drivers as reference, I have an lis2dtw12 that I want to use to detect 2 things:detect motion of any kind (and check the FIFO to confirm motion happened)detect a "drop" - eg "the consumer product was dropped and probably is ...

ATemp.1 by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos

Resolved! LPS25HB Temperature offset

Good day,I would like to know if it is possible to change the value of the temperature offset of the LPS25HB.If so what register will need to be manipulated?Thank you

CThir.1 by Associate
  • 1295 Views
  • 1 replies
  • 0 kudos

Resolved! LPS25HB Temperature compensation

Hi,Does the LPS25HB sensor automatically compensate for temperature ?If not how does one go about programming for it?Thank youCesar

CThir.1 by Associate
  • 1757 Views
  • 1 replies
  • 0 kudos

Resolved! LIS2DE12 interrup on wakeup

I have a simple task, to wake up the CPU when the device is shaken.It should be pretty simple, the MEMS sensor samples with 10Hz until I shake it, then it samples with 100Hz, but I get no interrupt. :(I use the driver form GIT hub and Interrupt INT1...

spa23 by Associate III
  • 3084 Views
  • 2 replies
  • 1 kudos

Resolved! How to stream data through serial port

Hi, I have purchased an STEVAL-MKI109V3 and the STEVAL-MKI207V1 (ISM330DHCX)I followed the instructions in section 4 in dm00331058-stevalmki109v3-professional-mems-tool-motherboard-for-mems-adapter-boards-stmicroelectronics.pdf to stream the dataIf I...

0693W00000DqPWNQA3.png 0693W00000DqPWSQA3.png
NAlwe.1 by Associate
  • 1861 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.