MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

accelerometer sensor current consumption

Hi,I am working on the lis2dh12 interface to MCU and getting the data. The below observations I found in our device.1. Getting x,y,z data2. The current consumption is taking 120ua.3. When I call the power down (Write LIS_CTRL_REG1, 0x00) it is carryi...

Akuma.6 by Associate III
  • 1591 Views
  • 1 replies
  • 0 kudos

Lis2 accelerometer sensor

Hi,​ I am looking lis2dh12 driver initialization with fall interrupt detection.​Please share sample program for understanding.​Regards,Kumar​

Akuma.6 by Associate III
  • 966 Views
  • 0 replies
  • 0 kudos

Resolved! "WHO_AM_I register value does not match the device selected"

My first time exploring with STEVAL hardware. I just received the STEVAL-MKI108V3 mother board, the STEVAL-MKI196V1 sensor board, and installed UNICO GUI 9.13.0 and FW Version V3.11.4. When starting the Unico Program with both "Automatic Port Detecti...

I3G4250D- PLLFILT required to be mounted for gyro to work

Hello, I am using the I3G44250D gyroscope without soldering the capacitors (C1=10nF,C2=470nF) and resistor (R2=10k) indicated for the PLLFILT, by using a configuration in which only the LPF1 filter is applied by default. With this configuration the g...

CMedi.1 by Associate
  • 978 Views
  • 0 replies
  • 0 kudos

Using FP-IND-PREDMINT1 for determining the frequency of vibration

Hello, I am using FP-IND-PREDMNT1 and new to this . From the data website it says it is used for time and frequency domain signal processing and analysis of 3D digital accelerometers with flat bandwidth up to 6 kHz. I wanted to know if is it possible...

PVaaz.1 by Associate III
  • 1854 Views
  • 2 replies
  • 0 kudos

Resolved! What is the accuracy of the LSM6DSO timestamp frequency of 40 KHz?

There does not seem to be anything in the datasheet about set tolerance, or drift over temperature.  https://www.st.com/resource/en/datasheet/lsm6dso.pdfAssume the INTERNAL_FREQ_FINE is unchanged. It has a step size of .15%, so one would presume the...

STEVAL-BLUEMIC-1 recording problem

Hi!I am using the STEVAL-BLUEMIC-1 to do wireless audio recordings, and I am noticing that the recordings get sped up. Is there a fix to this, or a reason why this may be happening?Thank you,Imran

IKalh.1 by Associate II
  • 871 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.