MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to resolve a STM32CubeProgrammer error: "Error: No STM32 target found!" while using a ST-Link/V2-lsol probe connected to a SensorTile.box eval board via the 20->14 pin adapter?

I have a SensorTile.box eval board connected to a ST-Link/V2-lsol using the 20->14 pin adapter. The ST-Link/V2 is connected to my linux workstation via USB and the ST-Link is seen by the STM32CubeProgrammer application. The SensorTile.box is also c...

dmcph.1 by Associate
  • 1662 Views
  • 1 replies
  • 0 kudos

IIS2DH Temperature data is not updating

I am working with the IIS2DH sensor. I can read all 3 axis data, but when I try to read the temperature I only got zeros. I read the similar forum threads, and I did not find a solution for my problem. I set the TEMP_CFG_REG(1F) to 0xC0, also set CT...

BLuka.1 by Associate
  • 919 Views
  • 0 replies
  • 0 kudos

53L1A1 SimpeRanging printf problem

Hello,I am working on the SimpleRanging example associated with X-NUCLEO-53L1A1 TOF sensor, so I lanched it using the IAR IDE as noted, but I can't read data in the Tera Term ( nothing is shown on the terminla) although I checked the IAR livewatch an...

WYous.1 by Associate III
  • 1636 Views
  • 2 replies
  • 0 kudos

LSM6DSO32 FIFO Reset

Hi,We are developing with the LSM6DSO32 in an application that experiences large shocks and during the shock we have found that the FIFO will contain a new timestamp and ODRCHG tag that is unexpected. A single timestamp and ODRCHG tag is consistent w...

Bobby123 by Associate II
  • 1191 Views
  • 0 replies
  • 0 kudos

reflectometer using a Time-of-Light VL53L0X

Hello Sir/ MadamI have a problem , and need your help I build the reflectometer step us below1) reflectometer using a Time-of-Light VL53L0X2) I can't see the bin file of VL53L0X_Reflectometer.bin_JEK (only see the VL53L1X)3) If I use the VL53L1X Refl...

Ahung.1 by Associate
  • 1814 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.