2023-08-02 2:32 AM
Hello. I made all the adjustments for my STEVAL kit. I also installed the necessary binary file in the Wifi module (Dsh predmnt). According to the guide I gave in the link, I stay on page 12 step 8. When I enter the wifi id password, it does not connect. My wifi module just lights up yellow red. Can you help me why the problem is caused?
I installed the DSH-PREDMNT binary file only on the wifi module. I did not install it on the STEVAL kit. could the problem be caused by this?
2023-08-03 3:32 AM
Hi @bcryhun ,
yes, you should first upload the STWIN with the FP-AI-PREDMNT2
then you can connect with wifi =)
If this answers your question, please, mark this as "best answer", by clicking on the "accept as solution" to help the other users of the community
Niccolò
2023-08-06 3:48 AM
it did not work. Clearly i am doing everything true. But when i try to write ssid and password of wifi, it does not respond. Documentation not clear.
2023-08-07 12:56 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.