MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Decoupling capacitor recommendations for ASM330LHH

Hi,Greetings!We are planning to use ASM330LHHTR in our design. As per the datasheet of Gyro sensor chip, it is recommended to have a decoupling capacitor of 0.1uF+10uF (Aluminum). Since we don't have enough space in our board to accommodate the Alumi...

Sa.11 by Associate II
  • 2670 Views
  • 1 replies
  • 0 kudos

How to give power supply to the IMU sensor ASM330LHB

The IMU sensor is  working on two input voltage supply 1.Vdd - Core supply 2.Vddio - digital I/O supply.My questions are in below.1.Is it better to supply the Vdd and Vddio seperately from two voltage regulators? 2.Is it better to supply the Vdd and ...

LSMDSO

Hi, Firstly, sorry for my low experiencia, i come here to try advanced in my project.I'm trying use the accelerometer LSMDSO with NUCLEO-F401RE and i i'm having difficult to read 3 axis data.Iam using the library present in the STM repository: https:...

Unico STEVAL-MKI230KA with NUCLEO-F401RE Board does not respond

I want to utilize the Unicode GUI for my ISM330IS Project, but my motherboard does not respond.. I've already updated the motherboard's firmware, tried different Unicode versions on Windows, and even checked the STink driver. Interestingly, Unicleo a...

Semolina by Associate II
  • 1873 Views
  • 1 replies
  • 0 kudos

Resolved! The WHO_AM_I register value does not match the device selected

Hi, I am using a STEVAL-MKI109V3 mother board to evaluate 2 accelerometers :LSM6DSOX (STEVAL-MKI197V1)LIS2DUXS12I want to use the GUI software UNICO v9.14.6.0 but when I want to connect my device, an error popup appear : "ERROR : The adapter board ha...

TZapp.1 by Associate II
  • 8542 Views
  • 16 replies
  • 0 kudos

Resolved! Unable to communicate with ICM-42688 P via SPI using STM32L412RB

I have a custom setup which contains a microcontroller STM32L412RB and a ICM-42688 P.I tried to communicate with the ICM-42688 P via SPI (4-wire, tried both 1MHz and 100kHz) using the command 0x75 to READ the WHO_AM_I register (thanks for implementin...

Dev_k by Associate II
  • 5217 Views
  • 2 replies
  • 0 kudos

Body Marking LSM6DSR

Hi ST Team, I have the body marking as below, but not sure under MPN#LSM6DSR or not? Seeking your support in checking on this case. Thank you in advance   Dai Nguyen

DaiNguyen_0-1699591665388.png

LSM6DS3TR-C behaviour

Hello...I'm currently testing the LSM6DS3TR-C sensor output before trying to proceed to calibration.I already run the internal self-test on the accelerometer and gyroscope, both results were between the acceptable range.After that I did my own tests ...

KevinSR by Associate II
  • 4144 Views
  • 5 replies
  • 0 kudos

Resolved! Behaviour change when powering with external power source

Hi everyone,I am using a STWINKT1B and I am trying to evaluate its power consumption while operating. The Wifi communication always works well when I power the board by the battery or the USB port but never when I plug it to my voltage source (5V on ...

chhhhak by Associate II
  • 3520 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.