Distance measured using LSM6DSO32TR
Hi, Could you provide any method/code to convert the acceleration values to distance(in cm)? we are able to read the acceleration but we need to know the distance covered as well. How to do it?
Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.
Hi, Could you provide any method/code to convert the acceleration values to distance(in cm)? we are able to read the acceleration but we need to know the distance covered as well. How to do it?
Does the Mems sensor LPS22HBTR require exercising before first use? Our company uses these for detectioopn of objects hitting a membrane and we have come to find out that it appears the mems sensor sometimes needs a puff of air in order to begin work...
Hello, IIS3DWB documentation provides only two data points about power consumption:Accelerometer current consumption @ 1.1mA typ.Accelerometer current consumption during power-down @ 5µA typ. I want to be woken-up on vibration levels (on X, Y or Z ax...
Hello . I have to boards L476RG and 303RE and of course IKS01A3 . After installing Unicleo , I can't connect to that IKS (It's not even showing port ) . I'm changing boards but still It can't see it . On some tutorials some lady was coping some file...
LIS2DE12용 Junction to Ambient, LGA-12 패키지의 열 저항이 필요합니다.
Hi all,I'm currently not able to read the temperature of my lis2de12.It always returns zero. lis2de12_temperature_meas_set(&dev_ctx, LIS2DE12_TEMP_ENABLE);lis2de12_data_rate_set(&dev_ctx, LIS2DE12_ODR_400Hz );lis2de12_block_data_update_set(&dev_ctx, ...
Hi Please can you advise on the Thermal Resistance (K/W) of LSM6DSOXTR please so we can complete our ATEx evaluation. Many Thanks Dominic
Hello,LIS2DH12 accelerometer. AN5005 datasheet. How is the data in the table in column 1 (Acceleration values) calculated? (See Figure 1). I read the calculation process in the datasheet above, but did not understand it. (See Figure 2).
Hi, I am reading from IMP34DT05 (master receive, PDM), and I always receive 0x00 0x7F 0xFF 0xFF ...and 0xFF's, ever after, until reset of SAI (disable-enable). Playing sound into mic has no effect. In debugger, immediately upon SAI enabled, FIFO is f...
Dear community,I am trying to detect metalic objects (train axles) that are passing above two LIS3MDL sensors. For this purpose I am using LIS3MDL breakout boards from PololuWhat I notice is that often, what seems randomly, the signal becomes noisy d...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.