MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ASM330LHH

hello,     i'm working on ASM330LHH IMU sensor, here raw value is continuously fluctuating even sensor is in untouch condition(fluctuation is between -1 to 6). is it possible to make it zero? so how can i stop this fluctuation. plz share suggetions o...

IIS2DLPC 6D orientation detection not working

Hi,I have attempted to follow the AN5201 application note page 26 to configure the IIS2DLPC accelerometer to generate an interrupt at every threshold however this interrupt is never generated. I have tried to print the value of SIXD_SRC register and ...

msingh08 by Associate III
  • 1309 Views
  • 1 replies
  • 0 kudos

Resolved! IIS3DWB - ODR Accuracy

Hello,I am working with the IIS3DWB for a vibration monitoring sensor, and have a few questions about the ODR (Output Data Rate) accuracy, hoping someone can help me.1. I know that on the datasheet the ODR accuracy is stated as +-1% typ, or +-2% Max....

Wellett by Associate
  • 2361 Views
  • 2 replies
  • 1 kudos

Resolved! SensorTile.box Pro and External Power Supply

Hi,I want to run an application for a week. This video says the battery life is 10 hours:https://youtu.be/gFkIcrUkP5w?t=452s Question:Can I use an external power supply like this and set it to 5v:https://www.adafruit.com/product/4880 Connect it's bar...

Williamx by Associate
  • 1461 Views
  • 1 replies
  • 0 kudos

Sensortile .Box Pro with H3LIS331DL accelerometer addon board

Hi,I have a Sensortile .Box Pro board and I plugged a H3LIS331DL high range accelerometer on its top socket.Is there any available code to log data from H3LIS331DL? I thought all MEMS evaulation boards from ST (STEVAL-MKI153V1 in this case) were supp...

iarakis by Associate II
  • 1465 Views
  • 1 replies
  • 0 kudos

Resolved! MTBF value for ASM330LHHTR

Hi,I am trying to calculate the MTBF (mean time between failures) value for the ASM330LHHTR module. Please suggest any techniques for the same. I am currently using the Qjc (Junction to Case Thermal Resistance) and Pd (Power Dissipation) values to ca...

Unico Merging of FSM and MLC

Hi ST Community,I currently have FSM and an MLC .ucf files. I have followed the instructions in DT0147 "Advanced design tips for the machine learning core and finite state machine using Unico-GUI", and have attempted to merge the FSM and MLC files in...

jspear by Associate II
  • 1820 Views
  • 1 replies
  • 0 kudos

How to calculate Altitude from Pressure read from LPS22HB sensor ?

I'm using Hypsometric formula to Calculate Altitude by using Pressure & Temperature. ( Source Code used to read the sensor https://github.com/stm32duino/LPS22HB )The Pressure value & Temperature are not in Sync.. Temperature Increases irrespective of...

TShet by Associate II
  • 3980 Views
  • 4 replies
  • 0 kudos

memsmic1 on P-Nucleo-WB55

Hello, I am trying to use the MEMSMIC1 example on my nucleo-wb55 board, specifically the microphones streaming exampe to record sounds with audacity. I am able to compile and run the code. I am also able to see the microphone show up in the device ma...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.