MEMS (sensors)

Ask questions and find answers on ST MEMS sensors, such as the LSM6DSV and the LSM6DSL. Learn how to use the SensorTile.Box, and STEVAL kits.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

MotionAC doesn't seem to be working.

Hi,I am trying to perform a 6-point tumble calibration for my LSM9DS1 accelerometer. The returned output data from the MotionAC_Update is always as follows:The "is_calibrated" parameter is always 0, indicating the accelerometer is not calibrated.The ...

0693W00000APNhrQAH.jpg
PMach.1 by Senior
  • 3782 Views
  • 5 replies
  • 0 kudos

Resolved! LIS2DS12TR Marking

We have received LIS2DS12TR, but we cannot identify the Marking of the Part.On the part there is a QR-Code and a "G". Could you please confirm that this is LIS2DS12TR and what the QR Code is standing for. Thank you in advance

Resolved! LSM6DSL gyroscope high-pass filter reset

Hi all,I have a question regarding the LSM6DSL's gyroscope high-pass filter configuration.For LSM6DS3, there is an option to reset the high-pass with HP_G_RST = 1. This way, the DC component of the angular velocity is immediately removed, c.f. https:...

flaufer by Associate II
  • 2164 Views
  • 2 replies
  • 1 kudos

Resolved! LIS344LH accelererometer

Good morning,I work actualy with the LIS344LH accelererometer and I was informed it will not be available anymore.Do you know any other devices that would substituate it ? I need it for measuring the movement of a tuning fork with a resonnance freque...

fru999 by Associate III
  • 1439 Views
  • 1 replies
  • 0 kudos

LPS22HH single/multiple Read on I3C

since LPS22HH support one byte read or multiple byte read. wonder how LPS22HH handles the last bit on I3C because last bit in Read data is 'T', rather than ACK/NACK from I3C Controller. How does LPS22HH (target) know Controller need single or mulitpl...

wenge by Associate
  • 875 Views
  • 0 replies
  • 0 kudos

6 pdm microphones with MEMSMIC1 example

Hello, I am currently running the MEMSMIC1 audio streaming example via usb with 4 channels and it works fine, but Because i am using the nucleo-wb55 board that has a pdm interface supporting up to 3 microphone pairs I want to use as many microphones ...

Resolved! LIS344ALH Pspice model

Hello everyoneI need to have the pspice model of LIS344ALH (i know that this product is not longer available)I try do it with the datasheet but i don't have enought infoCan someone help with it ? :)Thanks ;)

fru999 by Associate III
  • 2807 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.