2025-08-22 1:40 AM
It is recommended that CTRL9_XL DEVICE_CONF in ASM330LHH always set this bit to 1 when configuring the device, but when should it be set back to 0? Should it not be set back?
Solved! Go to Solution.
2025-08-28 6:31 AM
Hi @ggob ,
Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.
2025-08-28 6:31 AM
Hi @ggob ,
Once the device configuration is completed and stable, this bit can be set back to 0 if no further configuration changes are expected.
2025-08-28 4:54 PM
Thank you very much. This is very helpful.
Is it necessary to set this bit to “1” before setting it to “1” by operating BOOT or SW_RESET of CTRL3_C?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.