2022-06-14 6:02 AM
Hi,
We are trying to get Accelerometer without gravity
kindly let us know if there are any possible way to get the same.
Regards,
Dwithi
2022-06-14 6:46 AM
Put it on the Space Station.
I presume you mean eliminate the vertical G value. Subtract one G from the vertical reading. If the accelerometer rotates, use a version with a gyro output also and do the vector arithmetic to subtract the effect of gravity.
Cheers, Hal
2022-06-17 2:26 AM
kindly let us know with the calculation part.
2022-06-17 8:04 AM
This is your project. Do an Internet search on "axis rotation" and "axis transformation".
Cheers, Hal
2022-06-22 4:46 PM
enable the high pass filter on the chip, it will remove the dc offset (gravity)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.