2017-12-08 8:31 AM
I'm unclear about the the different types of interrupts generated by LIS2DE12 and similar devices.
In CTRL_REG3 (22h), the following interrupts can be enabled:
I understand what CLICK, WTM, and OVERRUN do, but I'm not completely sure about IA1, IA2, and ZYXDA. It appears that IA2 can be used for wake up interrupts defined by a threshold and duration, is that the same for IA1? What about ZYXDA?
I looked for app notes or other documentation that explain these interrupts, but I haven't found much so far.
Can someone point me to the appropriate document?
Thanks!
2017-12-09 1:34 AM
In CTRL_REG3 zou can configure which feature can generate interrupt on interrupt pin INT1.
I1_IA1 bit enable interrupt from Interrupt Generator 1 which can be configured by registers INT1_CFG, INT1_THS, INT1_DURATION.
I1_IA2 bit enable interrupt from Interrupt Generator 2 which can be configured by registers INT2_CFG, INT2_THS, INT2_DURATION.
I1_ZYXDA bit enable data ready interrupt, it means when new data are enable the interrupt is triggered.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.