2020-08-22 9:10 AM
Also, will the VBUS_EN_SNK pin get asserted (pulled low) in this case, allowing the power path to enable 5V from the USB 2.0 cable to power the device?
Solved! Go to Solution.
2020-08-26 7:26 AM
Hello,
yes. STUSB4500 connects to any USB-C source advertising properly as a DFP, whatever it support USB PD or only USB-C (5V only). In case a USB2.0 STD-A to C cable is used, it is recognised as a USB-C source with USB Default current capability (in case of USB 2.0, 500mA). Therefore, ATTACH pin is asserted. Concerning VBUS_EN_SNK pin, behaviour can be configured thanks to POWER_ONLY_ABOVE_5V option. By default, STUSB4500 powers the device, but for applications not supporting default 5V, it is possible to prevent the switch from closing for those cases when device is not attached to a PD compliant SOURCE (like USB2 STD-A port for instance).
Rgds
2020-08-26 7:26 AM
Hello,
yes. STUSB4500 connects to any USB-C source advertising properly as a DFP, whatever it support USB PD or only USB-C (5V only). In case a USB2.0 STD-A to C cable is used, it is recognised as a USB-C source with USB Default current capability (in case of USB 2.0, 500mA). Therefore, ATTACH pin is asserted. Concerning VBUS_EN_SNK pin, behaviour can be configured thanks to POWER_ONLY_ABOVE_5V option. By default, STUSB4500 powers the device, but for applications not supporting default 5V, it is possible to prevent the switch from closing for those cases when device is not attached to a PD compliant SOURCE (like USB2 STD-A port for instance).
Rgds
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.