2018-09-13 7:54 PM
BlueNRG-MS is initialized with CONFIG_DATA_MODE_OFFSET as Mode3 or Mode4, still fails.
BlueNRG-MS is initialized as GAP_CENTRAL_ROLE_IDB05A1.
BlueNRG-MS is not otherwise scanning or advertising or in a connection as a master or a slave.
Note that general scan works, so this
aci_gap_start_general_discovery_proc(192, 96, PUBLIC_ADDR, false);
returns success.
2018-09-16 11:28 PM
Hi Scott,
If only 1 connection is needed, it is not required to set Mode 1 or Mode 2 shall be fine.
Not sure what's wrong. The parameters you've given look valid to me.
Could you please try with BlueNRG GUI?
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.