2020-07-22 6:17 AM
Hi,
Bought the STM32 Nucleo kit w. USI Lora shield.
Disappointed when I found out that the documentation wasn't that great.
When using AT_Master or the End_Node example I dont find any options for retrieving the debug data.... Is the only option I have to spy on the TX/RX on the shield itself?
Or is it possible to retrieve the debug messages that is already in the examples?
BR,
Sindre
2020-07-22 6:29 AM
The USI module is a third-party implementation, with closed source.
An SWD header can be fitted, and the firmware can be replaced with relatively little porting effort. You can program/debug via an external ST-LINK attached to the header.
Not sure the USI module provides any additional diagnostic/debug information, review their data sheets and manuals.
For a richer experience I'd recommend the Discovery Board with the Murata module. It has a larger FLASH memory, and a newer radio chip, and would allow you to add as much diagnostic and telemetry as you need. Can support several UART and I2C
2020-07-22 6:45 AM
Wow @Community member ,
Fast answer :)
Ok, yeah I was ordering the wrong kit.
For some reason I believed that my order was with the MBed Lora shield not the USI one...
**** happens.
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.