Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USI STM32 Nucleo expansion board for LoRa

Hi,Bought the STM32 Nucleo kit w. USI Lora shield.Disappointed when I found out that the documentation wasn't that great.When using AT_Master or the End_Node example I dont find any options for retrieving the debug data.... Is the only option I have ...

SRavn.1 by Associate II
  • 1548 Views
  • 2 replies
  • 0 kudos

How to use stusb4500 get 15V without MCU?

Dear Team,I use stusb4500 and desgin this circuit,I connected type C with this circuit and measured VBus got 20V, then a few seconds later stusb4500 broke down.​Anything i have lost in this circuit then made it broke down? How to fix this circuit to ...

0693W000001rszXQAQ.png
YReya.1 by Associate
  • 1295 Views
  • 1 replies
  • 0 kudos

How to send commands over spi on the BlueNrg-MS

Hi everyone, I 'm on a project and sould developp a SPI communication between x-nucleo_idb05a1 and stm32F0 MCU and connect with a phone.The samples given on CubeMX are a bit complexes for what I have to do. I just want to send commands over SPI to in...

Yaya by Associate
  • 1236 Views
  • 1 replies
  • 1 kudos

Can someone kindly explain what are SPI_CS1 (e.g. DIO1), SPI_CS2 (e.g. DIO18), and SPI_CS3 (e.g. DIO19) on BlueNRG-2?

As far as I have understood, CS2 can be used for BlueNRG-2 acting as master and the another chip in salve mode, I can also see CS1 pin is also used for JTAG operation, does this mean CS1 can place BlueNRG-2 in slave mode for SPI communications? What ...

MAmiri by Associate II
  • 1385 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.