2021-12-22 1:34 AM
I am started to make with BlueNRG-LP based ble-project using WISE Studio IDE.
I choosed BLE SensorDemo example for our project.
But,
When compiling the example source, WISE Studio generates makefile only with the FIXED paths such as E:/Drivers/folder and E:/Middlewares/folder and try to build my example source.
So, I tried to find how to change the Fiexed path to my custom paths on my computer.
But I coudn't find it.
How can I change the path setting on WISE Studio IDE?
plz thanks in advance.
2022-01-28 3:35 AM
I hope that since then you've found the answer.
For anyone else looking:
Right click on the project -> Properties -> C/C++ Build -> Settings -> GCC C Compiler -> Includes
2022-01-30 6:27 AM
You're right.
Then I know what you said already and I tried it.
But it didn't work so I posted the issue before.
Still, it was left the problem to us.
2022-02-02 8:46 AM
Another thing that I was missing, but I believe was not the problem you are having (but again, posting just in case someone needed this info) was to add or modify the location of my resources:
Again in project -> Properties -> Resource -> Linked Resources -> Linked resources (this is a tab on the right hand window)
There you may add either by absolute or relative paths the location of the *.c files that are to be compiled and linked to your project.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.