2021-05-12 11:53 AM
Hello all,
I am attaching the schematics for a PD sink system we have designed and built. Our aim is to get this sink system to accept both PD and non PD type C power supplies and transfer their power to the 'FRONT_PWR' path on our schematics.
Of course a microcontroller is connected and controlling the PD parameters, etc. A few questions:
Thank you very much for your help!
Nir.
2023-08-04 11:20 AM
Hi,
Did you ever get an answer to your question, or figure out what was causing the shutdown?
I have a very similar situation, except at 20V.
2023-08-04 11:46 AM
Hi, I just realized I was using the STUSB4500L part, which is limited to 5V, as encountered by several others on the main thread. It looks like we want the part without the L.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.